35.5.2.4 Transceiver Delay Compensation
During the data phase of a CAN FD transmission only one node is transmitting, all others are receivers. The length of the bus line has no impact. When transmitting via pin CANx_TX the CAN receives the transmitted data from its local CAN transceiver via pin CANx_RX. The received data is delayed by the CAN transceiver’s loop delay. In case this delay is greater than TSEG1 (time segment before sample point), a bit error is detected. In order to enable a data phase bit time that is even shorter than the transceiver loop delay, the delay compensation is introduced. Without transceiver delay compensation, the bit rate in the data phase of a CAN FD frame is limited by the transceivers loop delay.
Description
The CAN’s protocol unit has implemented a delay compensation mechanism to compensate the transmitter delay, thereby enabling transmission with higher bit rates during the CAN FD data phase independent of the delay of a specific CAN transceiver.
To check for bit errors during the data phase of transmitting nodes, the delayed transmit data is compared against the received data at the Secondary Sample Point SSP. If a bit error is detected, the transmitter will react on this bit error at the next following regular sample point. During arbitration phase the delay compensation is always disabled.
The transmitter delay compensation enables configurations where the data bit time is shorter than the transmitter delay, it is described in detail in the new ISO11898-1. It is enabled by setting the DBTP.TDC bit (DBTP<23>).
The received bit is compared against the transmitted bit at the SSP. The SSP position is defined as the sum of the measured delay from the CAN’s transmit output CANx_TX through the transceiver to the receive input CANx_RX plus the transmitter delay compensation offset as configured by TDCR.TDCO bits (TDCR <15:8>). The transmitter delay compensation offset is used to adjust the position of the SSP inside the received bit (e.g. half of the bit time in the data phase). The position of the secondary sample point is rounded down to the next integer number of minimum time quantum (mtq). 1 mtq is equal to time period of GCLK_CANx clock.
The PSR.TDCV bits (PSR <22:16>) show the actual transmitter delay compensation value. PSR.TDCV bits (PSR <22:16>) are cleared when CCCR.INIT bit (CCCR <0>) is set and is updated at each transmission of an FD frame while DBTP.TDC bit (DBTP <23>) is set.
The following boundary conditions have to be considered for the transmitter delay compensation implemented in the CAN:
- The sum of the measured delay from CANx_TX to CANx_RX and the configured transceiver delay compensation offset FBTP.TDCR bits (TDCR <15:8>) has to be less than 6 bit times in the data phase.
- The sum of the measured delay from CANx_TX to CANx_RX and the configured transceiver delay compensation offset FBTP.TDCR bits (TDCR <15:8>) has to be less or equal to 127 mtq. In case this sum exceeds 127 mtq, the maximum value of 127 mtq is used for transceiver delay compensation.
- The data phase ends at the sample
point of the CRC delimiter, that stops checking of receive bits at the SSPs.
Transmitter Delay Compensation Measurement
If transmitter delay compensation is enabled by programming the DBTP.TDC bit (DBTP <23>) = ‘1’, the measurement is started within each transmitted CAN FD frame at the falling edge of bit FDF to bit res. The measurement is stopped when this edge is seen at the receive input CANx_TX of the transmitter. The resolution of this measurement is one mtq.
To avoid that a dominant glitch inside the received FDF bit ends the delay compensation measurement before the falling edge of the received res bit, resulting in a too early SSP position, the use of a transmitter delay compensation filter window can be enabled by programming TDCR.TDCF bit (TDCR <6:0>). This defines a minimum value for the SSP position. Dominant edges of CANx_RX, that would result in an earlier SSP position are ignored for transmitter delay measurement. The measurement is stopped when the SSP position is at least TDCR.TDCF bit (TDCR <6:0>) and CANx_RX is low.