13 Initiating a Page Erase
An individual page may be erased rather than erasing all of Flash memory. The PE is not used in this case.
PIC32MK family devices can perform an erase retry on a page by increasing the internal voltage used to perform the erase.
| Step Number | Op Code | Instruction |
|---|---|---|
| Step 1 | All the PIC32 devices: Initialize
constants. Registers a1, a2, and a3 are set for WREN =
1 or NVMOP[3:0] = 0100, WR =
1 and WREN = 1, respectively.
Registers s1 and s2 are set for the unlock data values and s0 is
initialized to ‘0’. | |
34054004 | ori a1, $0,0x4004 | |
34068000 | ori a2,$0,0x8000 | |
34074000 | ori a3,$0,0x4000 | |
3c11aa99 | lui s1,0xaa99 | |
36316655 | ori s1,s1,0x6655 | |
3c125566 | lui s2,0x5566 | |
365299aa | ori s2,s2,0x99aa | |
3c100000 | lui s0,0x0000 | |
| Step 2 | PIC32MX family devices only: Set register a0 to the base address of the NVM register (0xBF80_F400). | |
3c04bf80 | lui a0,0xbf80 | |
3484f400 | ori a0,a0,0xf400 | |
| Step 3 | PIC32MK and PIC32MZ family devices only: Set register a0 to the base address of the NVM register (0xBF80_0600). Register s3 is set for the value used to disable write protection in NVMBPB. | |
3c04b480 | lui a0,0xbf80 | |
34840600 | ori a0,a0,0x0600 | |
34138080 | ori s3,$0,0x8080 | |
| Step 4 | PIC32MK and PIC32MZ family devices only: Unlock and disable boot Flash write protection. | |
ac910010 | sw s1,16(a0) | |
ac920010 | sw s2,16(a0) | |
ac930090 | sw s3,144(a0) | |
00000000 | nop | |
| Step 5 | PIC32MK family devices only: Save the contents of NVMCON2. | |
8c9400a0 | lw s4,160(a0) | |
| Step 6 | PIC32MK family devices only: Set the initial programming voltage level and enable page testing (unlock required). | |
36953000 | ori s5,s4,0x3000 | |
32b5fcff | andi s5,s5,0xFCFF | |
| — | here3: | |
ac910010 | sw s1,16(a0) | |
ac920010 | sw s2,16(a0) | |
ac860008 | sw a2,8(a0) | |
ac9500a0 | sw s5,160(a0) | |
| Step 7 | All the PIC32 devices: Set the NVMADDR register with the address of the Flash page to be erased. | |
3c08<ADDR> | lui t0,<FLASH_PAGE_ADDR(31:16)> | |
3508<ADDR> | ori t0,t0,<FLASH_PAGE_ADDR(15:0)> | |
ac880020 | sw t0,32(a0) | |
| Step 8 | All the PIC32 devices: Poll the LVDSTAT register. | |
ac850000 | sw a1,0(a0) | |
| — | delay (6 us) | |
| Step 9 | PIC32MX devices only: Set up the NVMCON register for write operation. | |
| — | here1: | |
8c880000 | lw t0,0(a0) | |
31080800 | andi t0,t0,0x0800 | |
1500fffd | bne t0,$0,here1 | |
00000000 | nop | |
| Step 10 | All the PIC32 devices: Unlock the NVMCON register and start the write operation. | |
ac910010 | sw s1,16(a0) | |
ac920010 | sw s2,16(a0) | |
ac860008 | sw a2,8(a0) | |
| Step 11 | All the PIC32 devices: Loop until the WR bit (NVMCON[15]) is clear. | |
| — | here2: | |
8c880000 | lw t0,0(a0) | |
01064024 | and t0,t0,a2 | |
1500fffd | bne t0,$0,here2 | |
00000000 | nop | |
| Step 12 | All the PIC32 devices: Wait at least 500 ns after the WR bit (NVMCON[15]) clears before writing to any of the NVM registers. This requires inserting a delay in the execution. The programming tools and program executive utilizes the FRC 8 MHz clock. Therefore four NOP instructions equate to 500 ns(1). | |
00000000 | nop | |
00000000 | nop | |
00000000 | nop | |
00000000 | nop | |
| Step 13 | All the PIC32 devices: Clear the WREN bit (NVMCON[14]). | |
ac870004 | sw a3,4(a0) | |
| Step 14 | PIC32MK family devices only: Check that all data in the page has been erased. If not, adjust the voltage and try again. If all voltages levels have been tried, fail, and go to error procedure. | |
ac870004 | sw a3, 4(a0) | |
20171000 | addi s7, $0, 4096 | |
00005020 | add t2, $0, $0 | |
8c880020 | lw t0, 32(a0) | |
01194020 | add t0, t0, t9 | |
| — | here5: | |
8d090000 | lw t1, 0(t0) | |
15200005 | bne t1, $0, here6 | |
214a0010 | addi t2, t2, 16 | |
11570009 | beq t2, s7, here7 | |
00000000 | nop | |
1000fffa | beq $0, $0, here5 | |
21080010 | addi t0, t0, 16 | |
| — | here6: | |
22b50100 | addi s5, s5, 256 | |
32b60300 | andi s6, s5, 768 | |
16c0ffde | bne s6, $0, here3 | |
00000000 | nop | |
10000005 | beq $0, $0, err_proc | |
00000000 | nop | |
| Step 15 | PIC32MK family devices only: Restore the NVMCON2 register. | |
| — | here7: | |
ac9400a0 | sw s4,160(a0) | |
| Step 16 | All the PIC32 devices: Check the WRERR bit (NVMCON[13]) to ensure the successful completion of the program sequence. If an error occurs, jump to the error processing routine. | |
8c880000 | lw t0,0(a0) | |
30082000 | andi t0,t0,0x2000 | |
1500<ERR_PROC> | bne t0,$0,<err_proc_offset> | |
00000000 | nop | |
|
Note:
| ||