1.1.1.4.3 DRV_PLC_PHY_Close Function
C
void DRV_PLC_PHY_Close (
const DRV_HANDLE handle
);Summary
Closes an opened instance of the PLC PHY driver.
Description
This routine closes an opened instance of the PLC PHY driver, invalidating the handle.
A new handle must be obtained by calling DRV_PLC_PHY_Open before the caller uses the driver again.
Precondition
DRV_PLC_PHY_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Example
// 'handle', returned from DRV_PLC_PHY_Open previously called DRV_PLC_PHY_Close(handle);
Remarks
None.