1.1.1.4.9 DRV_PLC_PHY_ExceptionCallbackRegister Function
C
void DRV_PLC_PHY_ExceptionCallbackRegister (
const DRV_HANDLE handle,
const DRV_PLC_PHY_EXCEPTION_CALLBACK callback,
const uintptr_t context
);Summary
Allows a client to set an exception event handling function for the driver to call back when some error occurs through PLC transceiver communication.
Description
This function allows a client to register a PLC exception event handling function for the driver to call back when a communication SPI error occurs.
The event handler should be set before using the PLC transceiver in order to capture error events. The callback once set, persists until the client closes the driver or sets another callback (which could be a NULL pointer to indicate no callback).
Precondition
DRV_PLC_PHY_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| callback | Pointer to the callback function |
| context | The value of this parameter will be passed back to the client unchanged, when the callback function is called |
Returns
None.
Example
void APP_PLC_Exception_callback(DRV_PLC_PHY_EXCEPTION_OBJ *exceptionObj, uintptr_t context)
{
// The context handle was set to an application specific
// object. It is now retrievable easily in the event handler.
MY_APP_OBJ* myAppObj = (MY_APP_OBJ *) context;
// Exception handling here.
}
// myAppObj is an application specific state data object.
MY_APP_OBJ myAppObj;
// myHandle is the handle returned from DRV_PLC_PHY_Open API.
// Client registers a data confirm callback with driver. This is done once
DRV_PLC_PHY_ExceptionCallbackRegister( myHandle, APP_PLC_Exception_callback, (uintptr_t)&myAppObj );Remarks
None.