1.1.1.4.13 DRV_PLC_PHY_Tasks Function
C
void DRV_PLC_PHY_Tasks (
SYS_MODULE_OBJ object
);Summary
Maintains the driver's state machine.
Description
This function is used to maintain the driver's internal state machine.
Precondition
DRV_PLC_PHY_Initialize must have been called to obtain a valid system object handle.
Parameters
| Param | Description |
|---|---|
| object | Object handle for the specified driver instance (returned from DRV_PLC_PHY_Initialize) |
Returns
None.
Example
SYS_MODULE_OBJ object; // Returned from DRV_PLC_PHY_Initialize
while (true)
{
DRV_PLC_PHY_Tasks (object);
// Do other tasks
}Remarks
This function is normally not called directly by an application. It is called by the system's Tasks routine (SYS_Tasks).
This function will never block or access any resources that may cause it to block.