1.1.1.4.19 DRV_PLC_PHY_TX_CFM_CALLBACK Typedef
C
typedef void ( *DRV_PLC_PHY_TX_CFM_CALLBACK )( DRV_PLC_PHY_TRANSMISSION_CFM_OBJ *cfmObj, uintptr_t context );
Summary
Pointer to a PLC Driver Transmission Confirm Event handler function.
Description
This data type defines the required function signature for the PLC driver transmission confirm event handling callback function. A client must register a pointer using the callback register function whose function signature (parameter and return value types) match the types specified by this function pointer in order to receive transfer related event calls back from the driver.
Parameters
| Param | Description |
|---|---|
| cfmObj | Pointer to the object containing any data necessary to identify the result of the last transmission |
| context | Value identifying the context of the application that registered the event handling function |
Returns
None.
Example
void APP_MyTXCfmEventHandler( DRV_PLC_PHY_TRANSMISSION_CFM_OBJ *cfmObj, uintptr_t context )
{
MY_APP_DATA_STRUCT* pAppData = (MY_APP_DATA_STRUCT*) context;
switch(cfmObj->result)
{
case DRV_PLC_PHY_TX_RESULT_PROCESS:
// Transmission result: already in process
break;
case DRV_PLC_PHY_TX_RESULT_SUCCESS:
// Transmission result: end successfully
break;
case DRV_PLC_PHY_TX_RESULT_INV_LENGTH:
// Transmission result: invalid length error
break;
case DRV_PLC_PHY_TX_RESULT_BUSY_CH:
// Transmission result: busy channel error
break;
case DRV_PLC_PHY_TX_RESULT_BUSY_TX:
// Transmission result: busy in transmission error
break;
case DRV_PLC_PHY_TX_RESULT_BUSY_RX:
// Transmission result: busy in reception error
break;
case DRV_PLC_PHY_TX_RESULT_INV_SCHEME:
// Transmission result: invalid modulation scheme error
break;
case DRV_PLC_PHY_TX_RESULT_TIMEOUT:
// Transmission result: timeout error
break;
case DRV_PLC_PHY_TX_RESULT_INV_TONEMAP:
// Transmission result: invalid tone map error
break;
case DRV_PLC_PHY_TX_RESULT_INV_MODE:
// Transmission result: invalid G3 Mode error
break;
case DRV_PLC_PHY_TX_RESULT_NO_TX:
// Transmission result: No transmission ongoing
break;
}
}Remarks
If the result field is DRV_PLC_PHY_TX_RESULT_SUCCESS, it means that the data was transmitted successfully. Otherwise, it contains the transmission failure code.
The context parameter contains a handle to the client context, provided at the time the event handling function was registered using the DRV_PLC_PHY_TxCfmCallbackRegister function. This context handle value is passed back to the client as the context parameter. It can be any value necessary to identify the client context or instance (such as a pointer to the client's data) of the client that made the transfer add request.