SRV_PCOUP_Get_Config Function
C
SRV_PLC_PCOUP_DATA * SRV_PCOUP_Get_Config(void);
Summary
Get the PLC PHY Coupling parameters.
Description
This function allows to get the PLC PHY Coupling parameters. These parameters can be sent to the PLC device through PLC Driver PIB interface (DRV_PLC_PHY_PIBSet).
Precondition
None.
Parameters
None.
Returns
- Pointer to SRV_PLC_PCOUP_DATA Struct, containing the PLC PHY Coupling parameters.
Example
SRV_PLC_PCOUP_DATA *pCoupValues; pCoupValues = SRV_PCOUP_Get_Config();
Remarks
This function is only generated by MCC if the PLC driver uses Meters And More PHY.
If SRV_PCOUP_Set_Config function is used to set the PLC PHY Coupling parameters, this function is not needed.