SRV_PCOUP_Set_Config Function

C

bool SRV_PCOUP_Set_Config(DRV_HANDLE handle, SRV_PLC_PCOUP_BRANCH branch);

Summary

Set the PLC PHY Coupling parameters.

Description

This function allows to set the PLC PHY Coupling parameters, using the PLC Driver PIB interface (DRV_PLC_PHY_PIBSet).

Precondition

The PLC driver's open routine (DRV_PLC_PHY_Open) must have been called to obtain a valid opened device handle.

Parameters

ParamDescription
handleA valid instance handle, returned from the PLC driver's open routine.

Returns

  • true:
    • Successful configuration
  • false:
    • if there is an error when using the PLC driver PIB interface

Example

// 'handle', returned from DRV_PLC_PHY_Open or DRV_G3_MACRT_Open
bool result;

result = SRV_PCOUP_Set_Config(handle);

Remarks

This function is only generated by MCC if the PLC driver uses Meters And More PHY.