SRV_PCOUP_Set_Config Function

C

bool SRV_PCOUP_Set_Config(DRV_HANDLE handle, uint8_t phyBand);

Summary

Set the PLC PHY Coupling parameters for the G3-PLC PHY band.

Parameters

ParamDescription
handleA valid instance handle, returned from the PLC driver's open routine.
phyBandG3-PLC PHY band for which for which the parameters will be set.

Returns

  • true:
    • Successful configuration
  • false:
    • if phyBand parameter is not valid
    • if there is an error when using the PLC driver PIB interface

Example

// 'handle', returned from DRV_PLC_PHY_Open or DRV_G3_MACRT_Open
bool result;

result = SRV_PCOUP_Set_Config(handle, G3_FCC);

Remarks

This function is only generated by MCC if the PLC driver uses G3-PLC PHY.