1.2.5.4.2 SRV_PCRC_ConfigureSNA Function

C

void SRV_PCRC_ConfigureSNA
(
    uint8_t* sna
);

Summary

Sets SNA (Sub-Network Address) value to be used as initial value on further CRC calculations (used by PRIME stack).

Description

This routine sets the value that will be set as the initial CRC value for computations related to PRIME stack, as stated on PRIME specification.

Precondition

None.

Parameters

ParamDescription
snaPointer to buffer containing SNA value.

Returns

None.

Example

uint8_t sna[PCRC_SNA_SIZE];

SRV_PCRC_ConfigureSNA(sna);

Remarks

None.