1.1.4.2 DRV_METROLOGY_Reinitialize Function
C
Returns
SYS_MODULE_OBJ DRV_METROLOGY_Reinitialize (
SYS_MODULE_INIT * init
);SummaryRe-initializes the metrology driver according to the init parameter.
DescriptionThis routine re-initializes the metrology driver resetting the Coprocessor and its peripherals and re-loading the metrology library application on Core 1 from scratch. The initialization data is specified by the init parameter. It is a single instance driver.
Note: As described above, this routine resets the Coprocessor
peripherals. User must be aware of this if Main Processor is using peripherals
from Coprocessor, as they will require reconfiguration after
reset.
PreconditionThe low-level board initialization must have been completed and the module's initialization function must have been called before the system.
Parameters| Param | Description |
|---|---|
| init | Pointer to the init data structure containing any data necessary to initialize the driver. |
If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
ExampleSYS_MODULE_OBJ sysObjDrvMet;
extern uint8_t met_bin_start;
extern uint8_t met_bin_end;
/* Metrology Driver Initialization Data */
DRV_METROLOGY_INIT drvMetrologyInitData = {
/* MET bin destination address */
.regBaseAddress = DRV_METROLOGY_REG_BASE_ADDRESS,
/* MET Binary start address */
.binStartAddress = (uint32_t)&met_bin_start,
/* MET Binary end address */
.binEndAddress = (uint32_t)&met_bin_end,
};
sysObjDrvMet = DRV_METROLOGY_Initialize((SYS_MODULE_INIT *)&drvMetrologyInitData);RemarksNone.