1.1.4.38 DRV_METROLOGY_CALIBRATION Struct
C
typedefstruct {
DRV_METROLOGY_REGS_CONTROL metControlConf;
DRV_METROLOGY_CALIBRATION_REFS references;
uint32_t featureCtrl0Backup;
double freq;
uint32_t numIntegrationPeriods;
uint64_t dspAccIa;
uint64_t dspAccIb;
uint64_t dspAccIc;
uint64_t dspAccIn;
uint64_t dspAccUa;
uint64_t dspAccUb;
uint64_t dspAccUc;
int64_t dspAccPa;
int64_t dspAccPb;
int64_t dspAccPc;
int64_t dspAccPn;
int64_t dspAccQa;
int64_t dspAccQb;
int64_t dspAccQc;
int64_t dspAccQn;
bool running;
bool result;
} DRV_METROLOGY_CALIBRATION;SummarySpecifies all data internally needed for the auto calibration process.
DescriptionField description:
- metControlConf. Dummy variable used in internal computations.
- references. Calibration references. Client must be set the references before starting the calibration process.
- featureCtrl0Backup. Stores a backup value to restore FeatureCtrl0 register after finishing the calibration process.
- freq. Stores the mains frequency passed as parameter in the DRV_METROLOGY_SetConfiguration() routine.
- numIntegrationPeriods. Number of integration periods needed to complete the calibration process. It is set internally to 4.
- dspAccIa. Field internally used to perform the calibration process.
- dspAccIb. Field internally used to perform the calibration process.
- dspAccIc. Field internally used to perform the calibration process.
- dspAccIn. Field internally used to perform the calibration process.
- dspAccUa. Field internally used to perform the calibration process.
- dspAccUb. Field internally used to perform the calibration process.
- dspAccUc. Field internally used to perform the calibration process.
- dspAccPa. Field internally used to perform the calibration process.
- dspAccPb. Field internally used to perform the calibration process.
- dspAccPc. Field internally used to perform the calibration process.
- dspAccPn. Field internally used to perform the calibration process.
- dspAccQa. Field internally used to perform the calibration process.
- dspAccQb. Field internally used to perform the calibration process.
- dspAccQc. Field internally used to perform the calibration process.
- dspAccQn. Field internally used to perform the calibration process.
- running. Flag used to check if the calibration process was completed.
- result. Flag used to check if the calibration process has been successful.
None.