1.1.4.36 DRV_METROLOGY_CONFIGURATION Struct
C
typedefstruct {
uint32_t mc;
double freq;
double tr;
double rl;
uint32_t ku;
DRV_METROLOGY_SENSOR_TYPE st;
DRV_METROLOGY_GAIN_TYPE gain;
} DRV_METROLOGY_CONFIGURATION;
Summary
Identifies values needed to set different Metrology configuration parameters.
Description
Field description:
- mc. Meter Constant (amount of energy signified by one output pulse). Units: pulses/kWh (active energy), pulses/kVARh (reactive energy), or pulses/kAmp2-h (amp square).
- freq. Mains frequency. Units: Hz.
- tr.
- In the case of a current transformer, this is the current transformer ratio.
- In the case of a Rogowski Coil, this is the current sensitivity (units: μV/A) at the main frequency specified in Frequency parameter.
- rl.
- In the case of current transformer, this is the resistor load or burden resistor (units: Ω).
- In the case of shunt resistor, this is the shunt resistor value (units: μΩ).
- ku. Voltage divider ratio.
- st. Sensor Type. Refer to the DRV_METROLOGY_SENSOR_TYPE.
- gain. Programmable Gain Amplifier of the AFE (analog front end). Refer to the DRV_METROLOGY_GAIN_TYPE.
Remarks
None.