1.1.20.7.4 WDRV_WINC_MQTTUserPropSet
C
WDRV_WINC_STATUS WDRV_WINC_MQTTUserPropSet
(
DRV_HANDLE handle,
const uint8_t *pKey,
size_t lenKey,
const uint8_t *pValue,
size_t lenValue
)Description
Used to set or clear the value associated with a user property key.
Precondition
WDRV_WINC_Initialize must have been called.
WDRV_WINC_Open must have been called to obtain a valid handle.
WDRV_WINC_MQTTConnect must have been called to connect to a broker.
Parameters
| Parameters | Description |
|---|---|
| handle | Client handle obtained by a call to WDRV_WINC_Open. |
| pKey | Pointer to UTF-8 key name. |
| lenKey | Length of key name. |
| pValue | Pointer to UTF-8 value. |
| lenValue | Length of value. |
Returns
- WDRV_WINC_STATUS_OK - Request was accepted.
- WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open.
- WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
- WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
Remarks
Setting pValue to NULL or lenValue to zero will cause the user property key to be removed.