10.2.3.4 Allocation of Persist-attributed Sections
The persist section attribute specifies that a section
should be allocated as persistent storage in data memory, as defined by region
kseg0_data_mem and kseg1_data_mem in the linker
script. Persistent storage is not cleared or initialized by the C run-time library. The
following attributes may be used in conjunction with persist and will
further specify the allocation:
address()specifies an absolute addressnearspecifies the first 64 KB of data memoryalign()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1