10.2.3.1 Allocation of Code-attributed Sections
The code
section attribute specifies that a section
should be allocated in program memory, as defined by region
kseg0_program_mem
in the linker script. The following attributes may be
used in conjunction with code
and will further specify the allocation:
address()
specifies an absolute addressalign()
specifies alignment of the section starting address