10.2.3.2 Allocation of Data-attributed Sections
The data section attribute specifies that a section
should be allocated as initialized storage in data memory, as defined by regions
kseg0_data_mem and kseg1_data_mem in the linker
script. The following attributes may be used in conjunction with data and will further
specify the allocation:
address()specifies an absolute addressnearspecifies the first 64 KB of data memoryalign()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1