10.2.3.3 Allocation of Bss-attributed Sections
The bss section attribute specifies that a section should
be allocated as uninitialized storage in data memory, as defined by region
kseg0_data_mem and kseg1_data_mem in the linker
script. The following attributes may be used in conjunction with bss and
will further specify the allocation:
address()specifies an absolute addressnearspecifies the first 64 KB of data memoryalign()specifies alignment of the section starting addressreverse()specifies alignment of the section ending address + 1