5.7 Run Program Action
(Ask a Question)Program the PolarFire device with the bitstream which was generated in the previous step. To program the PolarFire device, perform the following steps:
- Ensure that the jumper settings on the board are listed in the following table.
Table 5-1. Jumper Settings for PolarFire Device Programming Jumper Description J18, J19, J20, J21, and J22 Short pin 2 and 3 for programming the PolarFire® FPGA through FTDI J28 Short pin 1 and 2 for programming through the on-board FlashPro Express J26, J27 Short pin 1 and 2 for programming through the FTDI SPI J39 Short pin 1 and 2 for enabling the Tx J4 Short pin 1 and 2 for manual power switching using SW3 - Connect the power supply cable to the J9 connector on the board.
- Connect the host PC to the J5 connector (FTDI port) on the board using a USB cable.
- Power on the board using the SW3 slide
switch.The following figure shows the PolarFire Evaluation Board setup for programming the device and running the reference design.
Figure 5-7. PolarFire Evaluation Board Setup - Double-click Run PROGRAM Action from the tab. When the device is successfully programmed, a green tick mark appears next to Run PROGRAM Action.