Note: The Power ON by UART Cmd option can be
used only when an external MCU controls the IS2083.
The following figure illustrates the UART interface between the IS2083 and an external
MCU. The external MCU can control the IS2083 over the UART interface and wake up the
module with the MFB and P0_0 pins.Figure 2-20. Host MCU Interface Over
UART
Perform the following steps to configure the power switch to power on using UART
command.
On the GUI tool initial page,
select “Host MCU Mode”.
From the Sys. Setup1 tab,
set the Power Switch Type as “Power ON by UART Cmd”.Figure 2-21. Power ON by UART Cmd
Option in GUI Tool
The following figures shows the timing sequence of Power ON/OFF. For more details, see
Host MCU Interface Over UART section in BM83 Bluetooth® Stereo Audio Module Data Sheet (DS70005402).