In this mode, IS2083 is powered ON when BAT_IN voltage is available and drives the Pulse
Gen Circuit to generate a pulse waveform on MFB pin (see the following figure). Figure 2-15. Power ON Directly
Circuit
Perform the following steps to configure the power switch to power ON directly.
On the GUI tool initial page,
select “Embedded Mode”.
Note: Selecting Host MCU Mode offers all three types of switch options. Selecting
Embedded Mode (without external MCU), supports only Power ON Directly and
MFB Power ON/OFF.
Figure 2-16. Embedded Mode Option
in GUI Tool
From the Sys. Setup1 tab,
set the Power Switch Type as “Power ON Directly”.Figure 2-17. Power Switch Setting
Options in GUI Tool