The user can power ON/OFF the power switch using a multifunction push button. A SW1 push
button is located between the SYS_PWR pin and the MFB pin. (See the following circuit.)
A pull-low resistor needs to be connected on the MFB pin.Figure 2-18. MFB Push Button Power Switch
Circuit
Perform the following steps to configure the power switch as MFB Power ON/OFF.
On the GUI tool initial page,
select “Embedded Mode”.
From the Sys. Setup1 tab,
set the Power Switch Type as “MFB Power ON/OFF”.Figure 2-19. MFB Push Button Power
Switch in GUI Tool