1.4.3 Selecting Next Bound Device
The SW17 QTouch key may be used to select a light. When this QTouch key is pressed and released, the next light becomes active, which means that all commands initiated by the user are sent to this light in a unicast manner. Groupcast mode will be entered automatically after twenty seconds. As soon as SW17 is pressed, the selected light will identify itself by blinking. If there are more than one LED load joined to the network, then LED loads will be selected in round robin manner.