4.8 Next Steps

After completing the installation of the tool chain and Harmony components as described in the Getting Started with Software Development section, the users can begin developing the application using the following documentation resources:

  1. BLE stack documentation: Guides the user on which API’s are required to implement wireless Bluetooth Low Energy application. For more details, refer to the BLE Software section of the MPLAB Harmony Wireless BLE.
  2. Zigbee stack documentation: Guides the user on which API’s are required to implement wireless Zigbee® application. For more details, refer to the BitCloud Zigbee Stack Architecture and API Overview section of the MPLAB Harmony Wireless BLE.
  3. Device support library documentation: It gives common system services like a device driver library and persistence data server library. These services are created as components in Harmony. For more details, refer to the PIC32CX-BZ3 Device Support Component Library Help section of the MPLAB Harmony PIC32CX-BZ System Services.
  4. BLE Application Example Documentation
  5. Adding Chip Peripherals to Application
  6. Zigbee Application Example Documentation