14.2.4.1.5 System Environment APIs
API functions of the System Environment component.
| Functions | |
| void | SYS_SubscribeToEvent (SYS_EventId_t id, SYS_EventReceiver_t
*recv) Subscribe a receiver to an event. The same receiver may be subscribed to multiple events by calling this function several times. |
| void | SYS_UnsubscribeFromEvent (SYS_EventId_t id, SYS_EventReceiver_t
*recv) Unsubscribe a receiver from an event. |
| void | SYS_PostEvent (SYS_EventId_t id, SYS_EventData_t data) Post an event to be delivered to all subscribed receivers. |
| bool | SYS_IsEventDeliverable (SYS_EventId_t id) Check if event have at least one subscriber. |
| bool | SYS_IsEventSubscriber (SYS_EventId_t id, SYS_EventReceiver_t
*recv) Check if the specified receiver is subscribed to an event. |
| void | SYS_ClearEvents (void) Clear the events. |
| bool | SYS_MutexLock (SYS_Mutex_t *const mutex, SYS_MutexOwner_t *const
owner) Makes the asynchronous request to lock the mutex. |
| bool | SYS_MutexUnlock (SYS_Mutex_t *const mutex, SYS_MutexOwner_t *const
owner) Unlocks a mutex using synchronous request. |
| bool | SYS_IsMutexLocked (SYS_Mutex_t *const mutex, SYS_MutexOwner_t *const
owner) Checks whether mutex is locked. |
| INLINE void | SYS_PostTask (SYS_TaskId_t taskId) Posts a task to the task manager, which is later processed by the task handler of the corresponding stack layer. |
| bool | SYS_RunTask (void) This function is called by the stack or from the
|
| SYS_InitStatus_t | SYS_SysInit (void) Initializes the microcontroller and the radio chip. |
| static uint16_t | SYS_GetRandomNumber (void) Generates a random two-bytes number. |
| uint16_t | SYS_GetNormalizedRandomNumber (uint16_t upperLimit) Generates a random two-bytes number normalized by given upper limit. |
| int | SYS_GetRandomSequence (uint8_t *buffer, unsigned long
size) Generates a sequence of random numbers and copies them into the buffer. |
| INLINE uint16_t | SYS_Crc16Ccitt (uint16_t initValue, uint8_t byte) Calculates CRC using CRC-16-CCITT algorithm. |