14.2.4.1.8 ZGP APIs
ZGP functions related to commission, control or get the information from the Green power device.
Some functions that are not intended to be used by the application but internally by the stack only are not listed.
| Functions | |
| void | ZGP_GetChannel(uint8_t *channel); Get zgp channel. |
| void | ZGP_ResetReq(ZGP_ResetReq_t *reqParams) To raise ZGP reset Req |
| void | ZGP_SetChannel(uint8_t channel) set zgp channel |
| void | ZGP_UnsubscribeCommissioning(void) This unsubscription will be used to deregister a commissioning callback, which will be used in Bidirectional commissioning |
| void | ZGPH_ProxyBasicInit(void) To initialize high proxy |
| ZGP_InfraDeviceStatus_t | ZGPH_PutLocalSinkInCommissioningMode(ZGP_SinkCommissioningModeOptions_t
*sinkCommModeOptions, uint8_t endPoint, bool unicastComm) To put local sink in commissioning mode. |
| void | ZGPH_SinkBasicInit(void) To initialize high sink |
| void | ZGPL_EnableDisableDirectMode(bool enabled) Enable/Disable direct mode to receive GPDF |
| void | ZGPL_FlushTxQueue(void) Flushout gpTxqueue |
| ZGP_Mode_t | ZGPL_GetDeviceMode(bool isProxy) To get the Device Mode (operational/Commissioning Mode) |
| void | ZGPL_GpdfDataRequest(ZGP_GpdfDataReq_t *zgpGpdfDataReq) GP-Data-Request(Raising from higher layer to dStub) |
| void | ZGPL_Init(void) Init. low zgp |
| void | ZGPL_KeyDerivationHmac(ZGP_SinkTableEntry_t* sinkTableEntry,
uint8_t *derivedKey, void (*keyedHashMacCb)(void)) To derive the GPD security key from network/group key. This is mainly used by high sink. |
| void | ZGPL_NvmTableInit(void) Initialize zgp NVM table |
| void | ZGPL_ResetTableEntry(void *entry, ZGP_EntryType_t tableType) To reset all the parameters of the given entry to init value |
| void | ZGPL_SendDeviceAnnounceCmd(uint16_t nwkAddr, uint64_t
extAddr) Sending device annce |
| void | ZGPL_SendSimpleDescReq(ShortAddr_t addr,uint8_t ep) To send simple descriptor request |
| void | ZGPL_SetDeviceMode(bool isProxy, ZGP_Mode_t mode) To set the Device in operational/Commissioning Mode |