1.3.4.1.12 FLAC_DecoderIsFileValid Function
C
bool FLAC_DecoderIsFileValid(void);
Summary
Function to check if a given FLAC file is valid or not, as per the supported features of this implementation.
Description
Returns true if the given file on which decoding is attempted is valid.
Precondition
FLAC_Initialize function must be called before this function.
Parameters
None.
Returns
bool - true if valid, else false.
Example
is_valid = FLAC_DecoderIsFileValid();
Remarks
None