1.3.4.1.8 FLAC_GetBlockSize Function
C
int32_t FLAC_GetBlockSize(void);Summary
Blocksize represents the number of samples in any of a block's subblocks. For example, a one second block sampled at 44.1KHz has a blocksize of 44100, regardless of the number of channels. This function returns that value.
Description
This function returns size of next packet to be decoded.
Precondition
FLAC_Initialize function must be called before this function.
Parameters
None.
Returns
Size of next packet to be decoded.
Example
blocksize = FLAC_GetBlockSize();
Remarks
None