Perform the following steps for Bluetooth initialization.
Double-click on
MCHPRT2.exe to open the GUI tool and select the device from the
drop down box.
Select the interface as “I2C” when
using “I2C” connection, and as “UART” when using serial bridge UART connection.
Select the Mode as BLE from the drop
down box, next to Mode.
Click Connect.Figure 2-14. Bluetooth
Initialization
The process bar status displays
Ready, after the initialization completes.
Navigate to BLE comport tab
under BLE.
Select the COM port number and, select Baud rate as 115200.
Click Open to connect to the
selected COM port.Figure 2-15. Selecting COM PortTo check if DTR is enabled, see UART/I2C Pin Details .
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.