5.4.1 Hexadecimal Communication
Perform the following steps for Hexadecimal communication.
- Enter the Hex command in the text box.
- Then double-click the input type display until
H
is shown. - Click ˄ to send the Hex command input manually.
Figure 5-13. Start Hexadecimal Communication 
- The sent manual input command is shown in the log.
- The log displays the format as
H
(Hexadecimal) orS
(String). Yellow represents the sent command [Hex] and Green represents the received command [Hex].Figure 5-14. Sent/Received Command 
Provide the Hexadecimal input with 1 byte (Min: 00, Max: FF). For example: 01 1E 20 03 00 00 00