26.6.1.1 DMA
The DMAC can transfer data between memories and peripherals without interaction from the CPU. The data transferred by the DMAC are called transactions, and these transactions can be split into smaller data transfers. The following figure illustrates the relationship between the different transfer sizes:
- Beat transfer – The size of one data transfer bus access, and the size is selected by writing the Beat Size bit group in the Block Transfer Control register (BTCTRL.BEATSIZE).
- Block transfer – The amount of data one transfer descriptor can transfer, and the amount can range from 1 to 64k beats. A block transfer can be interrupted.
- Transaction – The DMAC can link several transfer descriptors by having the first descriptor pointing to the second and so forth, as shown in Figure 26-2. A DMA transaction is the complete transfer of all blocks within a linked list.
A transfer descriptor describes how a block transfer must be carried out by the DMAC, and it must remain in SRAM (see Transfer Descriptors from Related Links).
The Figure 26-2 illustrates several block transfers linked together, which are called linked descriptors (see Linked Descriptors from Related Links).
A DMA transfer is initiated by an incoming transfer trigger on one of the DMA channels. This trigger can be configured to be either a software trigger, an event trigger or one of the dedicated peripheral triggers. The transfer trigger results in a DMA transfer request from the specific channel to the arbiter. If there are several DMA channels with pending transfer requests, the arbiter chooses which channel is granted access to become the active channel. The DMA channel granted access as the active channel will carry out the transaction as configured in the transfer descriptor. A current transaction can be interrupted by a higher prioritized channel, but resumes the block transfer when the related DMA channel is granted access as the active channel again.
For each beat transfer, an optional output event can be generated. For each block transfer, optional interrupts and an optional output event can be generated. When a transaction is completed, depending on the configuration, the DMA channel will either be suspended or disabled.