26.6.2.3 Transfer Descriptors
The transfer descriptors, together with the
channel configurations, decide how a block transfer must be executed. Before a DMA channel
is enabled (CHCTRLA.ENABLE is written to ‘1’) and receives a transfer
trigger, its first transfer descriptor must be initialized and valid (BTCTRL.VALID). The
first transfer descriptor describes the first block transfer of a transaction.
All transfer descriptors must reside in SRAM. The addresses stored in the Descriptor Memory Section Base Address (BASEADDR) and Write-Back Memory Section Base Address (WRBADDR) registers tell the DMAC where to find the descriptor memory section and the write-back memory section.
The descriptor memory section is where the DMAC expects to find the first transfer descriptors for all DMA channels. As BASEADDR points only to the first transfer descriptor of channel ‘0’ (see the following figure). All first transfer descriptors must be stored in a contiguous memory section, where the transfer descriptors must be ordered according to their channel number (see Linked Descriptors from Related Links).
The write-back memory section is where the DMAC stores the transfer descriptors for the ongoing block transfers. WRBADDR points to the ongoing transfer descriptor of channel ‘0’. All ongoing transfer descriptors are stored in a contiguous memory section where the transfer descriptors are ordered according to their channel number. The figure below shows an example of linked descriptors on DMA channel ‘0’ (see Linked Descriptors from Related Links).
The size of the descriptor and write-back memory sections are dependent on the number of the most significant enabled DMA channel m, as shown below:
For memory optimization, it is recommended to use the less significant DMA channels, if not all channels are required.
The descriptor and write-back memory sections can either be two separate memory sections, or they can share a memory section (BASEADDR=WRBADDR). The benefit of having them in two separate sections, is that the same transaction for a channel can be repeated without having to modify the first transfer descriptor. The benefit of having descriptor memory and write-back memory in the same section is that it requires less SRAM.