36.7.2 ADC Base Register (ADCBASE) Usage
After conversion of ADC is complete, if the interrupt is vectored to a function that is common to all analog inputs, it takes some significant time to find the ADC input by evaluating the ARDYx bits in the ADCDSTATx. To avoid this time spent, the ADCBASE register is provided, which contains the base address of the user’s ADC ISR jump table. When read, the ADCBASE register provides a sum of the contents of the ADCBASE register plus an encoding of the ARDYx bits set in the ADCDSTATx registers. This use of the ADCBASE register supports the creation of an interrupt vector address that can be used to improve the performance of an ISR.
The ARDYx bits are binary priority encoded with ARDY0 being the highest priority and ARDY11 being the lowest priority. The encoded priority result is, then, shifted left the amount specified by the number of bit positions specified by the IRQVS[2:0] bits in the ADCCON1 register, then, added to the contents of the ADCBASE register. If there are no ARDYx bits set, reading the ADCBASE register equals the value written into the ADCBASE register.
The ADCBASE register is typically loaded with the base address of a jump table that contains the address of the appropriate ISR. The kth interrupt request is enabled via the AGIENx bit (0-11) in ADCGIRQEN1.
When the ADC conversion for AN2 is complete, bit 2 of ADCDSTAT1 = ARDY2 is set.
Read value of ADCBASE = 0x1234 + (2 << 2) = 0x123C.
Therefore, the ISR must be placed at address 0x123C for AN2.