36.7.4 Individual and Global Interrupts
The use of the individual interrupts previously listed can significantly optimize the servicing of multiple ADC events by keeping each ISR focused on efficiently handling a specific event. In addition, different ISRs can be easily segregated according to the tasks performed, thereby making user software easier to implement and maintain. There may be cases where it is desirable to have a single ISR service multiple interrupt events. To facilitate this, each ADC event can be logically “ORed” to create a single global ADC interrupt. When an ADC event is enabled for a global interrupt, it vectors to a single interrupt routine. It is the responsibility of this single global ISR to determine the source of the interrupt through polling and process it accordingly.
Use of the Global Interrupt requires configuration of its own unique ISER, IPR0, INTFLAG and configuration of its interrupt vector as described in Interrupt Enabling, Priority and Vectoring. See Nested Vector Interrupt Controller (NVIC) from Related Links.
Interrupts for the ADC can be configured as individual or global or utilized as both where some are processed individually and others in the global ISR.