10.3.2 PHY-DATA.confirm
This data confirm callback executes the function set by the upper layer at the initialization of the PL360 Host Controller (see Setting Callbacks). It is called when a transmission request is processed. The format of the function is:
typedef void (*pf_data_confirm_t)(tx_cfm_t *px_msg_cfm);The result is reported in the following structure:
typedef struct tx_cfm {
uint32_t ul_tx_time;
uint32_t ul_rms_calc;
enum mode_types uc_mod_type;
enum tx_result_values uc_tx_result;
enum buffer_id uc_buffer_id;
} tx_cfm_t;Fields of the structure:
| ul_tx_time | Instant when frame transmission started, referred to the internal 1 μs PHY counter |
| ul_rms_calc | RMS_CALC value. It allows to estimate the voltage injected to the load |
| uc_mod_type | PRIME mode type (related constants defined in PHY-DATA.request) |
| uc_tx_result | Transmission result (related constants defined below) |
| uc_buffer_id | Identifier of the buffer used for transmission (related constants defined in PHY-DATA.request) |
Possible values of the field uc_tx_result are:
/* TX Result values */
enum tx_result_values {
TX_RESULT_SUCCESS = 1, /* Successful transmission */
TX_RESULT_INV_LENGTH = 2, /* Invalid length error */
TX_RESULT_BUSY_CH = 3, /* Busy channel error */
TX_RESULT_BUSY_TX = 4, /* Busy in transmission error */
TX_RESULT_INV_SCHEME = 6, /* Invalid modulation scheme error */
TX_RESULT_TIMEOUT = 7, /* Timeout error */
TX_RESULT_INV_BUFFER = 8, /* Invalid buffer identifier error */
TX_RESULT_INV_MODE = 9, /* Invalid PRIME Mode error */
TX_RESULT_CANCELLED = 11, /* Transmission cancelled */
TX_RESULT_HIGH_TEMP_120 = 12, /* High temperature (>120ºC) error (only with PL460) */
};