10.2.3 PHY-DATA.confirm
This data confirm callback executes the function set by the upper layer at the initialization of the PL360 Host Controller (see Setting Callbacks). It is called when a transmission request is processed. The format of the function is:
typedef void (*pf_data_confirm_t)(tx_cfm_t *px_msg_cfm);The result is reported in the following structure:
typedef struct tx_cfm {
uint32_t ul_rms_calc;
uint32_t ul_tx_time;
enum tx_result_values uc_tx_result;
} tx_cfm_t;Fields of the structure:
| ul_rms_calc | RMS_CALC value. It allows to estimate the voltage injected to the load |
| ul_tx_time | Instant when frame transmission ended, referred to the internal 1 μs PHY counter |
| uc_tx_result | Transmission result (related constants defined below) |
Possible values of the field uc_tx_result are:
/* TX Result values */
enum tx_result_values {
TX_RESULT_SUCCESS = 1, /* Successful transmission */
TX_RESULT_INV_LENGTH = 2, /* Invalid length error */
TX_RESULT_BUSY_CH = 3, /* Busy channel error */
TX_RESULT_BUSY_TX = 4, /* Busy in transmission error */
TX_RESULT_BUSY_RX = 5, /* Busy in reception error */
TX_RESULT_INV_SCHEME = 6, /* Invalid modulation scheme error */
TX_RESULT_TIMEOUT = 7, /* Timeout error */
TX_RESULT_INV_TONEMAP = 8, /* Invalid tone map error */
TX_RESULT_INV_MODTYPE = 9, /* Invalid modulation type error */
TX_RESULT_INV_DT = 10, /* Invalid delimiter type */
TX_RESULT_CANCELLED = 11, /* Transmission cancelled */
TX_RESULT_HIGH_TEMP_120 = 12, /* High temperature (>120ºC) error (only with PL460) */
};