3.7 Run Program Action
(Ask a Question)After generating the bitstream file, the PolarFire device must be programmed. Follow these steps to program the PolarFire device.
- Ensure that the jumper settings on the board are as listed in the following
table.
Table 3-2. Jumper Settings for PolarFire Device Programming Jumper Description J18, J19, J20, J21, and J22 Short pin 2 and 3 for programming the PolarFire FPGA through FTDI J28 Short pin 1 and 2 for programming through the on-board FlashPro Express J26 Short pin 1 and 2 for programming through the FTDI SPI J27 Short pin 1 and 2 for programming through the FTDI SPI J39 Short pin 1 and 2 for enabling the TX J4 Short pin 1 and 2 for manual power switching using SW3 - Connect the power supply cable to the J9 connector on the board.
- Connect the host PC to the J5 connector (FTDI port) on the board using a USB cable.
- Power on the board using the SW3 slide switch. The following
figure shows the PolarFire Evaluation Board setup for programming the device and running
the reference design.
Figure 3-6. PolarFire Evaluation Board Setup - Double-click Run PROGRAM Action from the tab. When the device is successfully programmed, a green tick mark appears next to Run PROGRAM Action, as shown in Figure 3-1.
For information about running the demo, see Running the Demo.