3.2 Place and Route
(Ask a Question)To place and route the design, TX_PLL, XCVR_REF_CLK and PF_XCVR must be configured using the I/O Editor. Follow these steps to configure the components and place and route the design:
- On the Design Flow window, double-click Manage Constraints.
- On the I/O Attributes tab, click Edit with I/O Editor, as shown in the following figure.
Figure 3-2. Edit with I/O Editor Option - Using the XCVR View in I/O Editor, place TX_PLL, XCVR_REF_CLK, and PF_XCVR TX as shown in the following figure.
Figure 3-3. I/O Editor Transceiver View When all the components are placed, the location of the components is updated in the
user_fp.pdcfile (located in tab), as shown in the following figure.Figure 3-4. Component Locations Updated in user_fp.pdc File 
- On the Design Flow window, double-click Place and Route.
- When place and route is successful, a green tick mark appears next to Place and Route, as shown in Figure 3-1.
- Right-click Place and Route and select View Report to view the place and route report and log files in the Reports tab. View the
top_place_and_route_constraint_coverage.xmlfile for place and route constraint coverage.