8.9.1 Wi-Fi Powersave
Wi-Fi Powersave state can be controlled by the kernel or the command line. To change
the default Powersave state,
CONFIG_CFG80211_DEFAULT_PS can be defined to
enable Powersave while the WLAN interface is being initialized, or undefined to disable
Powersave at initialization. To control Powersave manually after the WLAN interface is
initialized, use the iw tool.
$ iw dev wlan0 set power_save on
Note: The Powersave mode is disabled by default for
AP and P2P mode.