8.4 Modifying Configuration Files
To use the Wi-Fi module, the user must load a set of default configuration files on the prebuilt image. These files can be modified as per the requirement described in the following section.
To use the Wi-Fi module, the user must load a set of default configuration files on the prebuilt image. These files can be modified as per the requirement described in the following section.