5.8 WILC Support for Desired Kernel Version
By configuring the buildroot with
sama5d27_som1_ek_graphics_defconfig file, WILC Driver
support will be added to the kernel image that generate along with the buildroot
build and is available at
buildroot-at91/output/build/linux-linux4sam_6.2/. If the
user needs control on the kernel version, the user must download the new kernel
and build a new Image Tree Blob (.itb) file, and replace the
file present in the microSD Card.
.itb) file with WILC driver support is previously discussed
in Building the Component, the same
procedure is applicable here as well.