2.2 Design Checklist
(Ask a Question)The following table lists the various checks that design engineers must take care while designing the system.
| Guideline | Yes/No | Remarks |
|---|---|---|
| Prerequisites | ||
| See
PolarFire FPGA Datasheet
See UG0722: PolarFire FPGA Packaging and Pin Descriptions User Guide | ||
| See the board-level schematics of PolarFire Evaluation Kit. | ||
| Device Selection | ||
| Check for available device variants for
PolarFire FPGA. Select a device based on I/O pin count, transceivers, package, phase-locked loops (PLLs), and speed grade. | ||
| Check device errata in PolarFire Documentation. | ||
| Design Checklist | ||
| Power Analysis Download the PolarFire Power Estimator and check for the power budget. | ||
| Power Supply Checklist See Power Supplies for used power rails, and Figure 1-3 and Figure 1-4 for unused rails. | ||
| Decoupling Capacitors Follow PolarFire Decoupling Capacitors. Perform PI Analysis for any deviation from the recommended capacitors. | ||
| Clocks | ||
| For more information about dynamic phase
shift ports, see the “Dynamic Phase Shift Ports” table in
PolarFire Family Clocking Resources User Guide
. The XCVR reference clock ranges from 20 MHz to 400 MHz. | ||
The global clock network is driven by any of
the following:
For information about the preferred clock inputs connectivity to PLLs, DLLs, and global clock network, see the Packaging Pin Assignment Table (PPAT). High-Speed I/O Clocks High-speed I/O clock networks are driven by I/O or CCCs. The high-speed I/O clocks feed reference clock inputs of adjacent CCCs through hardwired connections. CCC The CCC is configured to have a PLL or DLL clock output, driving a high-speed I/O clock network. | ||
| Global Buffer (GB) is driven through the
dedicated global I/O, CCC, or fabric (regular I/O) routing. The global network
is composed of GBs to distribute low-skew clock signals or high-fanout nets. A dedicated global I/O drives the GBs directly and are the primary source for connecting external clock inputs (to minimize the delay) to the internal global clock network. For more information about global clock network, see PolarFire Family Clocking Resources User Guide . | ||
| Reset | ||
| For more information about DEVRST_N and user reset, see Reset. | ||
| DDR Interface | ||
| For more information about DDR routing and topology, see PolarFire Family Memory Controller User Guide . | ||
| Check Programming and Debugging Scheme. For programming and debugging information, see Device Programming. | ||
| XCVR | ||
| For more information about XCVR, see PolarFire Family Transceiver User Guide . | ||
| See the bank location diagrams in the PolarFire FPGA Packaging and Pin Descriptions User Guide to assess the preliminary placement of major components on PCB. | ||
| IOD | ||
| For I/O gearing interfaces, place the clocks and data based on the defined requirements by selecting the correct I/O. For more information about the placement of User I/O, see PolarFire FPGA and PolarFire SoC FPGA User I/O User Guide . | ||
| See the information about implementing Generic IOD Interface in PolarFire FPGA and PolarFire SoC FPGA User I/O User Guide . | ||
| See the Consolidated IOD Rules for pre-place and route guidance. |