1.1 Power Supplies

The following illustration shows the typical power supply requirements for PolarFire devices and the recommended connections of power rails when every part of the device is used in a system. For information on decoupling capacitors associated with individual power supplies, see PolarFire Decoupling Capacitors.

Figure 1-1. Power Supplies

To calculate the number of decoupling capacitors, it is important to know the target impedance of the power plane. Target impedance is calculated as follows:

Equation 1-1. Target Impedance
ZMax=% Ripple×VsupplyItrans

Where:

For the device to operate successfully, power supplies must be free from unregulated spikes and the associated grounds must be free from noise. All overshoots and undershoots must be within the absolute maximum ratings provided in the PolarFire FPGA Datasheet .

The following table lists the various power supplies required for PolarFire FPGAs.

Table 1-1. Supply Pins
NameDescription
XCVR_VREFVoltage reference for transceivers
VDD_XCVR_CLKPower to input buffers for the transceiver reference clock
VDDA25Power to the transceiver PLL
VDDA1Power to the transceiver TX and RX lanes
VSSCore digital ground
VDD2Device core digital supply
VDDI3 (JTAG Bank)Power to JTAG bank pins
VDDIx (GPIO Banks)Power to GPIO bank pins
VDDIx (HSIO Banks)Power to HSIO bank pins
VDD25Power to corner PLLs and PNVM
VDD18Power to programming and HSIO auxiliary supply
VDDAUXxPower to GPIO auxiliary supply
Note:
  1. VDDA: This supply can be powered to 1.0V or 1.05V. For more information, see tables 4-2 in PolarFire FPGA Datasheet . This is a quiet supply for the device. One method is to use a Linear regulator to ensure the supply is quiet.
  2. VDD: This supply can be powered to 1.0V or 1.05V. For more information, see tables 4-2 in PolarFire FPGA Datasheet .
VREFx: This is the reference voltage for DDR3 and DDR4 signals. The following VREF voltages can be generated internally and externally.
  • Internal VREF: This is not subjected to PCB and package inductance and capacitance loss. These changes provide the highest performance and can be programmed as required by DDR controller.
  • External VREF: This is fixed and cannot be programed as required. The PCB and package inductance and capacitance impact the VREF performance.
Important: If VDDI and VDDAUX need to be configured to the same voltage (2.5V or 3.3V), ensure both VDDI and VDDAUX are supplied from the same regulator. Do not use different regulators to source these rails. This prevents any voltage variations between VDDI and VDDAUX. In this case, the board must not supply the VDDI and VDDAUX from individual voltage supplies.

When a GPIO bank requires the VDDI to be less than 2.5V (1.2V, 1.5V, or 1.8V), the VDDAUX for that bank must be tied to 2.5V supply irrespective of the VDDI supply. The VDDI requires a separate supply for the specific I/O type (1.5V or 1.8V).

Important:
  • The on-chip Power-on Reset circuitry requires the VDD, VDD18, and VDD25 supplies to ramp monotonically from 0V to the minimum recommended operating voltage.
  • You must initiate the I/O calibration only when both the VDDA and XCVR_VREF supplies are up.

For a detailed pin description, see PolarFire FPGA Packaging and Pin Descriptions User Guide.