2.3 Libero Generated Files
(Ask a Question)Libero SoC software automatically generates the required files after stepping through the design entry steps of the transceiver. The following files are created:
- Netlist file—the RTL netlist instantiates the transceiver macros and related RTL wrappers based on protocol specific functions.
- <design name>.sdc file—Timing constraints file in the case of TXPLL and XCVR configurators.
- <module name>.v, _syn_comps.v, _pre_comps.v
- HDL source files for all Synthesis and Simulation tools.
- HDL source files for Synopsys SynplifyPro Synthesis tool.
- HDL source files for Mentor Precision Synthesis tool.
Note: The entire file list and their file paths are maintained in
mainfest.txt at <Project Directory>/component/work/<Component
name>/*_manifest.txt files.
Note: XCVR and PCIESS initialization data is available in the
generated netlists of the TXPLL, XCVR, and PCIE blocks. This is used to configure the
blocks specifically for users design customization. See Transceiver Initialization.