21.12.8 add_non_actel_device
(Ask a Question)Description
This Tcl command adds a non-Actel device in the chain. Either the file or (-tck and -ir) parameters must be specified. The Chain programming mode must have been set.
add_non_actel_device [-file "file"] \
[-ir "integer value"] \
[-tck "decimal value"] \
[-name "name"]
Arguments
Parameter | Type | Description |
---|---|---|
file | string | Specifies a BSDL file. |
ir | integer | Specifies the IR length. |
tck | integer | Specifies the maximum TCK frequency (in MHz). |
name | string | Specifies the device user name. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | You must either specify the 'file' or the 'ir' and 'tck' parameters. |
None | Parameter 'file' has illegal value. |
None | Parameter 'ir' has illegal value. |
None | Parameter 'tck' has illegal value. |
None | Parameter 'name' has illegal value. |
None | tck: Invalid argument value: '' (expecting decimal value). |
None | Parameter 'tck' must be greater than or equal to 1.000 |
None | Parameter 'tck' must be less than or equal to 100.000. |
None | ir: Invalid argument value: '' (expecting integer value). |
None | Parameter 'ir' must be greater than or equal to 2. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'add_non_actel_device [-file "file"] [-ir "integer value"] [-tck "decimal value"] [-name "name"]'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example adds {MyDevice} non actel device in the chain:
add_non_actel_device -ir {8} -tck {5} -name {MyDevice}