21.12.13 set_bsdl_file

Description

This Tcl command sets a BSDL file to a non-Microchip device in the chain. Chain programming mode must have been set. The device must be a non-Microchip device.

set_bsdl_file -name {device name} -file {path to the BSDL file}

Arguments

ParameterTypeDescription
namestringSpecifies the device name.
filestringSpecifies the BSDL file.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneParameter 'file' has illegal value.
NoneRequired parameter 'file' is missing.
NoneParameter 'name' has illegal value.
NoneParameter 'param_name' is not defined. Valid command formatting is 'set_bsdl_file -name "name" -file "file"'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4
SmartFusion® 2
IGLOO® 2

Example

The following example sets the BSDL file ./src/top.bsd to the device 'MyDevice':

set_bsdl_file -name {MyDevice} -file {./src/top.bsd}