Description
This Tcl command removes settings for non-Microchip or non-Actel device from the device
database.
remove_non_actel_device_from_database [-name {device name}]
Arguments
Parameter | Type | Description |
---|
name | string | Specifies the non-Actel or non-Microchip device name to be removed from the database. You can
repeat this argument for multiple devices. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'name' is missing. |
None | The device 'device_name' does not exist in the database. |
None | Parameter 'name' is missing or has invalid value. |
None | Parameter 'name' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'remove_non_actel_device_from_database [-name "name"]+'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example removes the "F1502AS" device from the database:
remove_non_actel_device_from_database -name {F1502AS}
See Also
- add_non_actel_device_to_database