21.12.1 add_actel_device

Description

This Tcl command adds an Actel device to the chain. Either the file or device parameter must be specified. Chain programming mode must have been set.

add_actel_device -name {name} \
                 [-file {filename}] \
                 [-device {device}]

Arguments

ParameterTypeDescription
namestringSpecifies the device user name. This parameter is mandatory.
filestringSpecifies a programming filename. This is an optional parameter.
devicestringSpecifies the device family (such as MPF300). This is an optional parameter.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneParameter 'name' has illegal value.
NoneYou must either specify the 'file' or the 'device' parameter.
NoneParameter 'param_name' is not defined. Valid command formatting is 'add_actel_device [-file "file"] [-device "device"] [-name "name"]'.
NoneParameter name is missing or has invalid value.
NoneParameter 'device' has illegal value.
NoneParameter 'file' has illegal value.
NoneEmpty file 'stp_file.stp'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4
SmartFusion® 2
IGLOO® 2

Example

This example adds "MPF300T" device with name "dev_name":

add_actel_device -device {MPF300T} -name {dev_name}