9.12.9 PolarFire SOC MSS I/O Attributes
(Ask a Question)These I/O attributes are valid only for MSS I/Os and are read only in the I/O Editor. These MSS I/O attributes appear on the right side of the default I/O attributes and will be visible even when there is no MSS being used in the design.
Reference Clock
The following table lists the MSS I/O attributes in the I/O Editor for Reference CLK.
MSS I/O Attributes | Values |
---|---|
MSS Resistor Pull | None, Up |
MSS Clamp Diode | OFF, ON |
MSS Persist | OFF, ON |
MSS User I/O Lock Down | OFF, ON |
MSS Odt (Ohm) | OFF, 100 |
MSS Thevenin (Ohm) | OFF, 150, 75, 50 |
MSS Schmitt Trigger | OFF, ON |
Peripheral I/Os
The following table lists the MSS I/O attributes in the I/O Editor for Peripheral I/Os.
MSS I/O Attributes | Values |
---|---|
MSS Resistor Pull | None, Up, Down, Hold |
MSS Clamp Diode | OFF, ON |
MSS Persist | OFF, ON |
MSS User I/O Lock Down | OFF, ON |
MSS Schmitt Trigger | Schmitt Trigger is always ON for 1.2, 1.5 and 1.8 V I/O Bank
values. Otherwise, it can be either ON or OFF. The MSS Schmitt
Trigger can have the following values: OFF, ON |
MSS Low Power Mode Input Receiver | OFF, ON |
MSS Low Power Mode Output Buffer | OFF, ON |
MSS Output Drive (mA) | 1.5, 2, 3, 3.5, 4, 6, 8, 10, 12, 16, 20, 24, 27, 30, 34, 40, 48, 60 |
DDR I/Os
The following table lists the MSS I/O attributes in the I/O Editor for DDR I/Os.
Based on the memory type used, the memory types have the following values.
Memory Type | Value |
---|---|
DDR3/DDR3L | 120, 60, 40, 30 |
DDR4 | 120, 80, 60, 40, 30 |
LPDDR3 | 240, 120, 80, 60, 40, 30 |
LPDDR4 | 120, 80, 60, 48, 40 |
Memory Type | Value (mA) |
---|---|
DDR3/DDR3L | 48, 34, 30, 24 |
DDR4 | 60, 48, 34, 27 |
LPDDR3 | 60, 48, 40, 34 |
LPDDR4 | 60, 48, 40, 34 |
SGMII I/Os
The following table lists the MSS I/O attributes in the I/O Editor for SGMII.
MSS I/O Attributes | Values |
---|---|
MSS Resistor Pull | None, Up, Down, Hold |
MSS Odt (Ohm) | OFF, 100 |
MSS Vcm Input Range | MID, LOW |
MSS Source Termination (Ohm) | OFF, 100 |
MSS Output Drive (mA) | 1.5, 2, 3, 3.5, 4, 6 |