3.6.1.3 Unroll Loop
(Ask a Question)- Syntax
#pragma HLS loop unroll factor(<int>)
- Description
- Specifies a loop to be unrolled. The factor indicates how many times to unroll the loop. If it is not specified, or specified as N (the total number of loop iterations), the loop will be fully unrolled. If it is specified as 2, the loop will be unrolled 2 times, where the number of loop iterations will be halved and the loop body will be replicated twice. If it is specified as 1, the loop will NOT be unrolled.
- Parameters
Parameter Value Optional Default Description factor
Integer Yes N (fully unroll) Unroll count - Position
- Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
- Examples
#pragma HLS loop unroll factor(1) for (int i = 0; i < 10; i++) { ... }